Company
Verifying SEL Software Downloads
Windows/Linux Software
Digitally signed software from selinc.com allows you to be sure that it is genuine (produced by SEL) and that it has not been altered or tampered with. Microsoft Windows users can check for and verify software digital signatures by using Windows Explorer. Here’s how:- Open Windows Explorer, and navigate to the folder containing the software file to be verified.
- Right-click the file, and select Properties from the menu that appears.
- Select the Digital Signatures tab. If you do not see a Digital Signatures tab, contact SEL customer service to obtain the information needed to verify the integrity and authenticity of the download.
- Click on the name of the signer in the Signature list.
- Click on the Details button.
- Verify that the name in the Signer information box is “Schweitzer Engineering Laboratories, Inc.” and that the Digital Signature Details message says, “This digital signature is OK.”
Blueframe Software
To verify that Blueframe software downloads are genuine—produced by SEL and not altered or tampered with—users can compare the SHA-256 hashes on the downloaded files with the SHA-256 hashes listed on the Latest Software Versions webpage. Windows users can check the SHA-256 hash on OS and package files by using Command Prompt. Here's how:- Launch the Windows Command Prompt.
- Utilize the certUtil command, which is a built-in Windows command for generating the SHA-256 hash. Ensure the root directory matches where your file is saved and issue the following command, replacing with the correct path:
certUtil -hashfile SHA256
- When complete, the SHA-256 hash will be displayed. Verify that this SHA-256 hash matches what is provided by SEL on the Latest Software Versions webpage.