Schweitzer Engineering Laboratories

Newsroom

Jul 30, 2025

SEL enhances the performance and digital input capacity of the SEL-2240 Axion

PULLMAN, Washington—Schweitzer Engineering Laboratories (SEL), a global leader in power system protection, automation and control solutions, announces two new modules for the SEL-2240 Axion.

The first addition is the SEL-2241-2 Real-Time Automation Controller (RTAC) Module, which delivers over five times the processing power of the prior-generation RTAC module. This matches the performance of the popular SEL-3350 computing platform, but in a smaller, modular form factor. As an all-in-one intelligent electronic device, the higher processing power makes common functions like bay control, power system monitoring and digital fault recording more responsive as single- or multiple-use applications.

The second addition is the SEL-2244-4 Digital Input Module, which brings 33 percent more digital input capacity than the previous-generation digital input module. This increased capacity allows customers to streamline their system monitoring infrastructure and easily replace multiple high-I/O legacy remote terminal units or bay controllers with minimal wiring changes. To learn more about enhancements to the Axion, visit selinc.com/mktg/do-more-with-the-sel-2240-axion-rtac.

Back to Newsroom 
Featured Stories

SEL In The News

Inventing the future: An interview with Dr. Ed Schweitzer

SEL In The News

Tariffs are harming manufacturing. Congress must act now

Technical

SEL Website Improves Navigation With New Sections for Products, Industries, and Services

  • How two SEL employees turned a simple fix into a patented solution
  • Pursuing patents a regular routine for SEL

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow