Solution
GSE partnered with SEL to develop a country-wide emergency control system (ECS) to keep the power system stable. SEL exceeded GSE’s requirements by designing an ECS that can react to a power system event in less than 12 milliseconds. The GSE and SEL team specified, designed, built, tested, and installed the entire system in under four months.The ECS solution includes decision-making SEL relays at the most critical transmission line substations. These relays constantly monitor the transmission lines, check for faults, and quickly shed loads if a fault occurs. This prevents overload in other areas of the power system to maintain stability and prevent blackouts. Results
The effectiveness of the new ECS was proven in the summer of 2011 when, in a two-week period, it was called upon five times to shed loads at 500 kV substations along The Backbone. The SEL system worked as designed, protecting the country from blackouts and ushering in a new era of reliable energy for the Republic of Georgia.GSE has continued to work with SEL to improve reliability ever since. Following the initial ECS success, GSE asked SEL to help create a remedial action scheme (RAS) to further improve reliability, system management, and fault recovery. Soon after, GSE called on SEL again to modernize the protection, control, monitoring, and communications systems for ten GSE substations. This modernization greatly improved the capabilities and resilience of the substations. In addition, the SEL design and construction methods enabled the project to be completed in just two years—half of the alloted time.One step at a time, GSE’s efforts are paying off, and life is looking much brighter in Georgia.