Automation News

54 results

Aug 21, 2025

A new set of Real-Time Automation Controller (RTAC) human machine interface (HMI) tagged templates is now available to enhance workflow.

Aug 8, 2025

Learn how the RTAC R155-R201 firmware enhances Axion substation monitoring capabilities.

Jul 30, 2025

SEL is releasing two new modules for the SEL-2240 Axion: the upgraded SEL-2241-2 Real-Time Automation Controller (RTAC) Module and SEL-2244-4 Digital Input Module. The new SEL-2241-2 RTAC now contains the same CPU as the popular SEL-3350 RTAC. The SEL-2244-4 is a new 32 digital input module that increases the total digital I/O and offers new combinations to support product retrofits.

Apr 29, 2025

We’ve recently released enhancements to applications in SEL Blueframe, including Resource Management, Direct Resource Access, and the Data Management and Automation (DMA) application suite.

Apr 3, 2025

We are updating the Real-Time Automation Controller (RTAC) product line with new features and adding a 64-bit version of the RTAC OS. These updates add power quality measurement capabilities to the SEL-2240 Axion, enhance interoperability with devices from other vendors, and upgrade cybersecurity features by supporting SNMPv3.

Feb 24, 2025

Larger SSD makes SEL computers and select RTACs more effective in storage-heavy applications.

Oct 31, 2024

We’ve added 32 new DI/DO status LEDs to SEL-3350 3U RTACs ordered with a DI/DO expansion board.

Oct 10, 2024

Easily monitor and manage alarms on-site.

Sep 27, 2024

SEL Axion modules now stream synchrophasor data at 120 messages per second.

Sep 27, 2024

We’ve added a new use for session IDs created in the Resource Management application on Blueframe that makes it easier to securely connect to a device.

Sep 25, 2024

The latest RTAC firmware update includes new alarm functionality for Axion Bay Controller touchscreens, a tag selector tool for acSELerator RTAC SEL-5033 Software, automated network event capture, and more.

Sep 16, 2024

Collect system-wide metering data using the Data Management and Automation (DMA) application suite on the SEL Blueframe application platform.

Aug 15, 2024

With a last-time buy date set for acSELerator Team, read our recommendation for smoothly transitioning to its successor, the DMA application suite on SEL Blueframe.

May 7, 2024

Upgrading to an SEL-3300 series automation and computing platform becomes easier with the newly released SEL-2902 RJ45 to DB-9 Adapter Panel.

Apr 4, 2024

The SEL-2414 Transformer Monitor now offers a five-inch color touchscreen option, an enhanced processor, and IEC 61850 enhancements.

Mar 29, 2024

The SEL-3355-2 computing platform is now VMware-certified. We’ve also released a VMware-certified driver for the SEL-3390E4 Ethernet card.

Feb 27, 2024

Built-in redundancy for SEL Blueframe minimizes downtime during unexpected failures or system upgrades. The feature is currently available for Blueframe virtual machine deployments and will soon become available for deployments on SEL computing platforms.

Dec 11, 2023

RTAC Firmware version R152 is now available and includes Continuous Recording Groups, Grid Connect enhancements, and more.

Nov 22, 2023

Support added for backup reciprocating generators and islanded power management, new library extension coming soon

Page 1 of 3