Software Downloads


Search
Categories
Model
Results
(41)

SEL-3355 Device Drivers and System Software

The SEL-3355 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3355. Please read the installation instructions and release notes that are included in each download prior to installation.

SEL-3355 Drivers and Software, All

This package contains all SEL-3355 device drivers and software that are included on the DVD that is included with the SEL-3355 in the factory packaging. Most 64-bit Windows operating systems are fully supported, while some 32-bit Windows and Linux operating systems are only partially supported (no SEL SysMon or Watchdog support). Contact SEL if you have questions about support for a specific operating system.

Size 504.64 MB
Date Code 20170315

Verifying SEL Software Downloads

SEL-3355 SATA Link Power Management Patch

This patch disables link power management, a power conservation function that is known to cause reliability issues with some solid-state drives (SSDs). Link power management provides little power-saving benefit in SEL-3355 Computers, and disabling the function has no negative impact on SEL-3355 operation. This patch is only applicable to SEL-3355 Computers with Windows operating systems in which the Intel serial ATA (SATA) driver is installed.

Size 969.00 B
Date Code 20150409

Verifying SEL Software Downloads

SEL USB Driver

This driver enables USB communication between Windows computers and SEL USB ports.

Installation Instructions

  1. Ensure USB device is not plugged in.
  2. Download and open R6.6.0.0.Driver.exe.
  3. Click Yes when prompted to Install SEL USB to UART Drivers.
  4. Click Next when finished with installation.
  5. Restart computer.
  6. Plug in the USB cable.
  7. Wait for the PC to finish the installation.
  8. To see new COM port assignment, open Device Manager and expand Ports.

Notes

Download this driver to communicate with USB ports on the following devices:

  • SEL-2440
  • SEL-3031
  • SEL-C662
  • SEL-C663
  • SEL-C667
  • SEL-3021
  • SEL-9192
  • SEL-T4287
For 32-bit and 64-bit Windows 8, Windows 7, Vista, and XP operating systems.

Version R6.6.0.0
Size 3.55 MB
Date Code 20130215

Verifying SEL Software Downloads

SEL-3355 Firmware and BIOS Updates

These updates provide enhancements, bug fixes, and security updates to the firmware and BIOS embedded in the SEL-3355 system. Please read the installation instructions and release notes that are included in each download prior to installation.

SEL-3355 B2071 BIOS Update

This package contains the files necessary to update the BIOS in the B2071 mainboard used in the SEL-3355 computer. This update contains a number of enhancements, see the included ReleaseNotes.txt file for details. 

Size 504.64 MB
Date Code 20170315

Verifying SEL Software Downloads

SEL-3355 Intel Management Engine (ME) Firmware Update

This package includes the Intel Management Engine firmware and update tools as provided by Intel. It contains the latest security updates and bug fixes at the time of this release, notably CVE-2017-5689. This update is not included in the BIOS update package and must be installed to ensure your computer's firmware is fully up to date. 

Version 8.1.71.3608
Size 13.87 MB

Verifying SEL Software Downloads

SEL-3332 Operating System Updates

Contains updates and modifications to the operating system environment. Please install any missing updates in the order in which they were released and carefully follow instructions if included with the update you download.

Microsoft Windows Security Updates (Spring 2017)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2017). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from July 2016 through June 2017, and includes the MS17-010 (KB4012598) Security Update previously released for the SEL-3332.

Microsoft Windows Security Updates (Spring 2016)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2016). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2016 through June 2016.

Microsoft Windows Security Updates (Fall 2015)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from July 2015 through December 2015.

Size 115.79 kB
Date Code 20160225

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2015)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2015 through June 2015.

Version SEL-3332 R304 versions
Size 22.87 MB
Date Code 20150805

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2014)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from June 2014 through December 2014.

Version SEL-3332 R304 versions
Size 15.58 MB
Date Code 20150226

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2014)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from October 2013 through May 2014.

Version SEL-3332 R304 versions
Size 15.61 MB
Date Code 20141002

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2013)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2013). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from May 2013 through October 2013.

Version SEL-3332 R304 versions
Size 55.26 MB
Date Code 20131227

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2013)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily July 2012 through May 2013. This update also updates the Foxit Reader.

Version SEL-3332 R304 versions
Size 68.78 MB
Date Code 20130731

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2012)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily November 2011 through June 2012. This update also installs the latest version of Foxit Reader.

Version SEL-3332 R304 versions
Size 36.63 MB
Date Code 20120827

Verifying SEL Software Downloads

MS12-020 Security Update (KB2621440)

Updates SEL-3332 R3.0.4 systems with Microsoft's Remote Desktop Security Update KB2621440.

Version SEL-3332 R3.0.4 VERSIONS ONLY
Size 605.88 kB
Date Code 20120402

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2011)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily April 2011 through November 2011 as well as some older, lower priority Microsoft Security Updates. This update also installs the Foxit Reader instead of Adobe Reader.

Version SEL-3332 R304 VERSIONS
Size 52.48 MB
Date Code 20120125

Verifying SEL Software Downloads

Microsoft Windows Security Updates (April 2011)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily August 2010 through April 2011 as well as some older, lower priority Microsoft Security Updates. We have also included two relevant Security Updates from Adobe Systems Incorporated.

Version SEL-3332 ALL VERSIONS
Size 83.73 MB
Date Code 20110525

Verifying SEL Software Downloads

Microsoft Windows Security Updates (August 2010)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering January 2010 through August 2010. This update addresses the vulnerability discussed in NERC R-2010-09-13-01 (MS10-046).

Version SEL-3332 ALL VERSIONS
Size 41.16 MB
Date Code 20101022

Verifying SEL Software Downloads

Microsoft Windows Security Updates (January 2010)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering August 2009 through January 2010.

Version SEL-3332 ALL VERSIONS
Size 19.72 MB
Date Code 20100301

Verifying SEL Software Downloads

MS08-067 Security Update (KB958644)

Updates all OS revisions with Microsoft's Patch Security Update KB958644.

Version SEL-3332 ALL VERSIONS
Size 616.23 kB
Date Code 20081027

Verifying SEL Software Downloads

Protected Storage sub-system Update (R3.0.3)

Updates OS revision 3.0.2 with an updated protected storage sub-system.

Version SEL-3332 OS R3.0.3
Size 7.94 MB
Date Code 20151102

Verifying SEL Software Downloads

Daylight-Saving Time Update (R3.0.2)

Updates OS revision 3.0.1 to handle the change to daylight-saving time that phases in March 11, 2007.

Version SEL-3332 OS R3.0.2
Size 485.12 kB
Date Code 20070207

Verifying SEL Software Downloads

SEL-3354 Security Updates

Contains updates and modifications to the operating system environment. Please install any missing updates in the order in which they were released and carefully follow instructions if included with the update you download.

Microsoft Windows Security Updates (Spring 2017)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2017). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2016 through June 2017, and includes the MS17-010 (KB4012598) Security Update previously released for the SEL-3354.

Version SEL-3354 with Windows Embedded Standard
Size 66.35 MB

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2016)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2016). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from June 2016 through December 2016.

Version SEL-3354 with WindowsEmbedded Standard
Size 83.18 MB

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2016)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2016). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2016 through June 2016.

Version SEL-3354 with WindowsEmbedded Standard
Size 51.50 MB

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2015)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from July 2015 through December 2015.

Version SEL-3354 with Windows Embedded Standard
Size 61.63 MB
Date Code 20160225

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2015)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2015 through June 2015. This update also includes a security update from Adobe.

Version SEL-3354 with Windows Embedded Standard
Size 101.17 MB
Date Code 20150805

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2014)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from May 2014 through December 2014. This update also includes security updates for Adobe Reader and Silverlight.

Version SEL-3354 with Windows Embedded Standard
Size 218.78 MB
Date Code 20150226

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2014)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from October 2013 through May 2014. This update also includes security updates for Adobe Reader and Silverlight.

Version SEL-3354 with Windows Embedded Standard
Size 135.55 MB
Date Code 20141002

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2013)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2013). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from May 2013 through October 2013. We have also included relevant Security Updates from Adobe® Systems Incorporated.

Version SEL-3354 with Windows Embedded Standard
Size 79.13 MB
Date Code 20131227

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2013)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily July 2012 through May 2013. This update also includes security updates for Adobe Reader and Silverlight.

Version SEL-3354 with Windows Embedded Standard
Size 111.05 MB
Date Code 20130731

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2012)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily November 2011 through June 2012. This update includes security updates for a few non-Operating System supporting software such as Adobe Reader and Silverlight.

Version SEL-3354 with Windows Embedded Standard
Size 291.61 MB
Date Code 20120827

Verifying SEL Software Downloads

MS12-020 Security Update (KB2621440)

Updates all WES SEL-3354 with KB2621440.

Version SEL-3354 with Windows Embedded Standard
Size 621.98 kB
Date Code 20120402

Verifying SEL Software Downloads

Microsoft Windows Security Updates (November 2011)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily May 2011 through October 2011 as well as some older, lower priority Microsoft Security Updates. We have also included relevant Security Updates from Adobe Systems and the new .NET 4 Framework for Windows Embedded Standard.

Version SEL-3354 with Windows Embedded Standard
Size 474.51 MB
Date Code 20111123

Verifying SEL Software Downloads

Microsoft Windows Security Updates (April 2011)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily August 2010 through April 2011 as well as some older, lower priority Microsoft Security Updates. We have also included two relevant Security Updates from Adobe Systems Incorporated.

Version SEL-3354 with Windows Embedded Standard
Size 114.28 MB
Date Code 20110531

Verifying SEL Software Downloads

Microsoft Windows Security Updates (August 2010)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable installer covering January 2010 through August 2010. This update addresses the vulnerability discussed in NERC R-2010-09-13-01 (MS10-046).

Version SEL-3354 with Windows Embedded Standard
Size 50.05 MB
Date Code 20101022

Verifying SEL Software Downloads

SEL-3354 Silverlight

4.0.60531.0

This version of Silverlight for Windows Embedded Standard will update your current Silverlight 4.X version to 4.0.60531.0.

Version 4.0.60531.0
Size 5.99 MB
Date Code 20110830

Verifying SEL Software Downloads

SEL-3354 Ethernet Port

Microsoft Windows Ethernet Port Intel Teaming Upgrade

This package configures the rear ethernet ports to enable Intel Advanced Network Services (ANS) functionality, such as Teaming. This is only applicable to systems manufactured after May 2011 (serial number 1111350000 and higher). See the included readme.txt file for more information.

Version 1.1.49152.1
Size 40.74 MB
Date Code 20141216

Verifying SEL Software Downloads

Ubuntu Linux (64-bit) Ethernet Port Configuration

This package configures the rear ethernet ports to force 100Mbit Full Duplex operation. This should be applied to systems that have Fiber Optic rear ethernet ports, or when connected to network devices that do not support auto negotiation of speed and duplex.

Version Ubuntu Linux (64-bit)
Size 6.54 kB

Verifying SEL Software Downloads

Ubuntu Linux (32-bit) Ethernet Port Configuration

This package configures the rear ethernet ports to force 100Mbit Full Duplex operation. This should be applied to systems that have Fiber Optic rear ethernet ports, or when connected to network devices that do not support auto negotiation of speed and duplex.

Version Ubuntu Linux (32-bit)
Size 6.54 kB

Verifying SEL Software Downloads

SEL-3351 Operating System Updates

Contain updates and modifications to the operating system environment. Please install any missing updates in the order in which they were released and carefully follow instructions if included with the update you download.

MS08-067 Security Update (KB958644)

Updates all OS revisions with Microsoft's Patch with Security Update KB958644.

Daylight-Saving Time Update (R1.0.2)

Updates OS revisions 1.0.0—1.0.1 to handle the change to daylight-saving time that phases in March 11, 2007.

Version SEL-3351 OS R1.0.2
Size 520.00 kB
Date Code 20070207

Verifying SEL Software Downloads

System Control Monitor Updates

Contain updates to the watchdog, alarming, and time-acquisition processes.

Version R1.0.0.13
  SystemMonitor 1.1.1.2
  SystemControlMonitor 1.1.1.0
Size 602.00 kB
Date Code 20060110

Verifying SEL Software Downloads

SEL-3360 Device Drivers and System Software

The SEL-3360 requires device drivers and software to be installed on the operating system in order for the devices such as Ethernet, video, audio, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3360. Please read the installation instructions and release notes that are included in each download prior to installation.

SEL-3360 B2071 Drivers and Software

This package contains all SEL-3360 device drivers and software that are included on the DVD that is included with the SEL-3360 in the factory packaging. Most 32-bit and 64-bit Windows operating systems are fully supported. Windows XP and some Linux operating systems are only partially supported (no SEL SysMon or Watchdog support). Contact SEL if you have questions about support for a specific operating system.

Size 504.64 MB
Date Code 20170315

Verifying SEL Software Downloads

SEL-3360 SATA Link Power Management Patch

This patch disables link power management, a power conservation function that is known to cause reliability issues with some Solid State Drives (SSDs). Link power management provides little power saving benefit in SEL-3360 Computers, and disabling the function has no negative impact on SEL-3360 operation. This patch is only applicable to SEL-3360 Computers with Windows operating systems in which the Intel serial ATA (SATA) driver is installed.

Size 969.00 B
Date Code 20150409

Verifying SEL Software Downloads

SEL-3351 Device Driver and System Software

The SEL-3351 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3351.

SEL-3351 Drivers and Software, All

This package contains all SEL-3351 device drivers and software that are included on the CD that is included with the SEL-3351 in the factory packaging. Windows XP is fully supported, and some versions of Linux are also supported. Contact SEL if you have questions about support for a specific operating system.

Size 13.52 MB
Date Code 20140307

Verifying SEL Software Downloads

SEL-1102 Device Driver and System Software

The SEL-1102 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-1102.

SEL-1102 Drivers and Software, All

This package contains all SEL-1102 device drivers and software that are included on the CD that is included with the SEL-1102 in the factory packaging. Windows XP is fully supported, and some versions of Linux are also supported. Contact SEL if you have questions about support for a specific operating system.

Size 13.52 MB
Date Code 20140307

Verifying SEL Software Downloads

SEL-3354 Device Driver and System Software

The SEL-3354 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3354.

SEL-3354 Drivers and Software, All

This package contains all SEL-3354 device drivers and software that are included on the DVD that is included with the SEL-3354 in the factory packaging. Windows XP, 7, and Server 2008R2 are fully supported, and some versions of Linux are also supported. Contact SEL if you have questions about support for a specific operating system. 

Size 848.02 MB
Date Code 20160721

Verifying SEL Software Downloads

SEL-3354 IRIG Driver

This package contains the installation files for the SEL-3354 IRIG Driver.

Version 1.1.4.0
Size 59.13 MB
Date Code 20160715

Verifying SEL Software Downloads

SEL-3354 Firmware Updates

These updates provide enhancements, bug fixes, and security updates to the firmware embedded in the SEL-3354 system. Please see the instruction manual Appendix A for release notes.

SEL-3354 Firmware, Windows

This file updates the SEL-3354 firmware to the latest release for use with Microsoft Windows operating systems.

Version 1.1.3.0
Size 5.78 MB
Date Code 20140528

Verifying SEL Software Downloads

SEL-3354 Firmware, Linux

This file updates the SEL-3354 firmware to the latest release for use with Linux operating systems.

Version 2.0.3.0
Size 531.03 kB
Date Code 20110411

Verifying SEL Software Downloads

SEL-5056 Flow Controller

The SEL-5056 Flow Controller is enterprise software based on Microsoft Windows Server and designed to optimize SDN configuration and management for critical infrastructure. The SEL-5056 Flow Controller is designed to work collectively with the SEL-2740S SDN Switch to provide a complete traffic-engineering solution for Ethernet-based LANs. Traffic engineering with the SEL-5056 Flow Controller enables flexible configuration of each communications flow path and the ability to proactively engineer fault-tolerant networks, resulting in greater performance, improved reliability, and more deterministic packet delivery.

SEL-5056 Flow Controller

Version 1.3.0.0
Size 90.24 MB

Notes

You can download and use the SEL-5056 Flow Controller free of charge to manage up to four OpenFlow switches. Contact SEL to purchase a license for more than four switches. Chrome 52 or higher is required to operate this software.

Release Date: 1/11/2018

Verifying SEL Software Downloads

acSELerator QuickSet SEL-5030 Software

acSELerator QuickSet SEL-5030 Software is a tool for engineers and technicians to quickly and easily configure, commission, and manage devices for power system protection, control, metering, and monitoring. QuickSet Device Manager, included as a free, optional expansion pack, provides additional device management, control, and versioning capabilities.

Full Install

Version 6.6.1.1
Size 1.09 GB
Date Code 20171219

Verifying SEL Software Downloads

Last supported version for Windows XP

Version 5.17.0.2
Size 581.84 MB
Date Code 20150112

Verifying SEL Software Downloads

SEL Compass

SEL Compass goes beyond basic software updates to provide, among other offerings, a rich selection of meaningful literature, application guides, and general software products. Use the enhanced sorting capabilities to facilitate product planning, organize and distribute information, and learn about the many products SEL provides.

Full Install

Version 3.0.5.1
Size 127.13 MB
Date Code 20171021

Verifying SEL Software Downloads

acSELerator Architect Software

Substation communications networks using the IEC 61850 MMS and GOOSE protocols require a systemic methodology to configure message publications and subscriptions. acSELerator Architect SEL-5032 Software is a Microsoft Windows application that streamlines the configuration and documentation of IEC 61850 control and SCADA communications.

Full Install

Version 2.2.24.0
Size 221.43 MB
Date Code 20180129

Verifying SEL Software Downloads

acSELerator RTAC Software

acSELerator RTAC is a graphical, easy-to-use tool that helps users quickly and easily configure the SEL-3530 Real-Time Automation Controller (RTAC).

Full Install

Version 1.24.141.14170
Size 771.79 MB
Date Code 20171204

Verifying SEL Software Downloads

Library Extensions

Version 3.17.11.4
Size 13.61 MB
Date Code 20171121

Verifying SEL Software Downloads

acSELerator Diagram Builder Software

The SEL Real-Time Automation Controller (RTAC) family of devices supports an optional web-based human-machine interface (HMI) system that is well-suited for use in substations and small processes. acSELerator Diagram Builder SEL-5035 Software is a Microsoft Windows application that enables the creation and management of HMI visualization projects for all of the RTACs in your system.

Diagram Builder

Version 3.2.5.698
Size 24.14 MB
Date Code 20180209

Verifying SEL Software Downloads

RTAC HMI Runtime Files

Version 3.2.5.698
Size 76.88 MB
Date Code 20180209

Verifying SEL Software Downloads

SEL-5806 Curve Designer Software

SEL-387E Relay Volts/Hertz User Curve Design Software.

Full Install

Version 1.3.0.0
Size 584.00 kB
Date Code 20160526

Verifying SEL Software Downloads

SEL-5020 Settings Assistant Software

Enter settings to and communicate with your SEL communications processors. Use to create a template for a new device.

Full Install

Version 3.60.3.0
Size 14.37 MB
Date Code 20110809

Verifying SEL Software Downloads

SEL-5010 Relay Assistant Software

Communicate with and manage SEL Relays across your system.

Full Install

Version 4.36.1.0
Size 70.91 MB
Date Code 20100202

Verifying SEL Software Downloads

PDC Assistant Software

The SEL PDC Assistant software provides quick and easy commissioning for the SEL-5073 software PDC as well as SEL-3573 and SEL-3373 hardware PDCs.  Make settings in online or offline mode, monitor system status, export diagnostic logs and archives, and manage user accounts.

Full Install

Version 2.3.0
Size 76.92 MB
Date Code 20170711

Verifying SEL Software Downloads

acSELerator Team SEL-5045 Software

acSELerator Team automates the collection of power system data from multiple devices and stores these data in a central location for easy access. 

Trial downloads: Please read the Team_IS_TeamTrial.pdf document found in the extracted contents of the download for additional information.

Installs

Version DDC, EDT, TMS: 1.38.2.0; Sync: 2.2.24.1; Excel Templates: 1.0.12.0; Web Server: 1.0.0.0
Size 500.81 MB
Date Code 20180102

Verifying SEL Software Downloads

synchroWAVe Event Relay Event Visualization And Analysis Software

SEL-5601-2 synchroWAVe Event Software helps engineers diagnosis a protective relay’s behavior during a power system fault. It is a powerful yet easy-to-use solution for displaying and analyzing SEL relay event reports and COMTRADE files.

Full Install

Version 1.4.0.396
Size 104.00 MB
Date Code 20171115

Verifying SEL Software Downloads

acSELerator Meter Reports SEL-5630 Software

SEL meters help you monitor electric load profiles and power quality across your system. You can combine SEL meters with pulse-type or DNP3-enabled devices to monitor consumption of other resources, such as water, air, gas, and steam. Team automatically retrieves and stores metering data on these resources in a centralized database.

Meter Reports enhances the visualization and analysis of data captured by SEL meters in your system. After Team collects and stores the data from the metering devices, Meter Reports displays the information so that you can drive planning, operating, and accounting decisions that will increase efficiency and reduce costs.

This version of acSELerator Meter Reports requires acSELerator Database version 2.0.18.0 or higher. Please verify that your system is up to date or contact SEL support for assistance: +1.509.338.3838

 

Full Install

Version 1.0.7.0
Size 137.78 MB
Date Code 20170530

Verifying SEL Software Downloads

acSELerator Report Viewer SEL-5042 Software

Efficiently Analyze Event Reports at Your PC.

Full Install

Version 1.33.1.0
Size 13.63 MB
Date Code 20080318

Verifying SEL Software Downloads

acSELerator Report Server SEL-5040 Software

Reduce time retrieving reports and analyzing system events.

SEL recommends that customers use acSELerator Team SEL-5045 Software instead of the acSELerator Report Server SEL-5040 Software.

Full Install

Version 2.41.1.0
Size 10.39 MB
Date Code 20100519

Verifying SEL Software Downloads

SEL-5078-2 synchroWAVe Central

synchroWAVe Central Software provides power system situational awareness by translating data into visual information. It’s a powerful solution for the display and analysis of time-synchronized synchrophasor data and relay event reports.

Notes

synchroWAVe Central requires both synchroWAVe Historian and Services to be installed

synchroWAVe Historian Install

Version 2.0.3.491
Size 52.84 MB
Date Code 20170524

Verifying SEL Software Downloads

synchroWAVe Services Install

Version 2.0.3.491
Size 140.55 MB
Date Code 20170524

Verifying SEL Software Downloads

SubstationSERVER.NET

V1.51 SEL-3332 - Update from v1.38

DUA update package for use with the SEL-3332 Intelligent Server. Upgrades from v1.38 to v1.51.

Version 1.51
Size 39.19 MB
Date Code 20101001

Verifying SEL Software Downloads

V1.51 SEL-3332 - Update from v1.32

DUA update package for use with the SEL-3332 Intelligent Server. Upgrades from v1.32 to v1.51.

Version 1.51
Size 37.07 MB
Date Code 20101001

Verifying SEL Software Downloads

SEL-3378 SVP Configurator

Version 1.0.0.0
Size 63.52 MB
Date Code 20140805

Verifying SEL Software Downloads

SEL-5401 Test Software for SEL-4000

Full Install

Version 1.0.0.7
Size 2.51 MB
Date Code 20110223

Verifying SEL Software Downloads

SEL-5801 Cable Selector

Quickly and easily select proper SEL cables for your various applications. The SEL-5801 Cable Selector helps you select the right cable, with a user interface and database of standard SEL cables. The Cable Selector is available as a free download.

Full Install

Version 3.0.5.0
Size 6.02 MB
Date Code 20061227

Verifying SEL Software Downloads

SEL-5860 Clock Software

Connect SEL clocks to PCs with Windows for accurate computer time.

Notes

 32 bit64 bit
XP
Server 2003 (R2)
Server 2008 (R2) 
Server 2012 
Windows 7
Windows 8
Full Install

Version 2.0.0.11
Size 52.27 MB
Date Code 20141103

Verifying SEL Software Downloads

SEL-5891 Data Courier Configurator

Configure the SEL-4391 Data Courier.

Notes

The SEL-4391 is no longer available for purchase.

English Version

Version 1.0.5.0
Size 668.00 kB
Date Code 20100303

Verifying SEL Software Downloads

Español Version

Version 1.0.5.0
Size 804.00 kB
Date Code 20100303

Verifying SEL Software Downloads

SEL RxTx BLUETOOTH Application for Mobile Devices

This App allows mobile devices to use BLUETOOTH communications technology to communicate with SEL-2924 Portable BLUETOOTH Serial Adapters and SEL-2925 BLUETOOTH Serial Adapters, that are in turn connected to the serial ports of host devices.

Notes

Example host devices include (but are not limited to) meters, protective relays, real-time automation controllers, programmable automation controllers, recloser controls, capacitor bank controls, voltage regulator controls, control computers, annunciators, programmable logic controllers, valve controls, spillgate controllers, security gate systems, building control and security systems, HVAC systems, and more.

SEL RxTx for Android 2.1 and higher

Version 1.0.0.0
Size 126.35 kB
Date Code 20121009

Verifying SEL Software Downloads

SEL RxTx for Blackberry OS 7.x

Version 1.0.0.0
Size 56.65 kB
Date Code 20121009

Verifying SEL Software Downloads

acSELerator Analytic Assistant SEL-5601 Software

Display oscillograms and vector diagrams to analyze event reports from SEL relays and COMTRADE files. 

Full Install

Version 2.3.23.0
Size 6.33 MB
Date Code 20130222

Verifying SEL Software Downloads

SEL-5025 Secure Port Service

Secures serial communications using the SEL-3045 and SEL-3055

Notes

Version information: Released April 12, 2016. Corrected issue with service not starting on Windows 10.

Full Install

Version 1.0.1.22
Size 6.63 MB
Date Code 20160316

Verifying SEL Software Downloads

SEL-3060 Discovery Tool

This Windows-based tool is designed to easily find SEL-3060 Ethernet Radios and set their IP addresses. From the SEL-3060 Discovery Tool, users can connect to each device webpage for configuration of wireless settings.

Notes

The SEL-3060 Discovery Tool is designed for use with SEL-3060 Ethernet Radios only.

For 32-bit and 64-bit Windows Vista, Windows 7, Windows 8, and 64-bit Windows XP operating systems.

SEL-3060 Discovery Tool

Version 1.0.0.0
Size 484.00 kB
Date Code 20131210

Verifying SEL Software Downloads

SEL Backup and Recovery Tool (BaRT)

Quickly and easily create a snapshot of your computer’s operating system and configuration with SEL BaRT. SEL BaRT was designed specifically for SEL’s rugged computer line and takes advantage of each platform’s features, including the system watchdog, which is responsible for monitoring system availability.

SEL BaRT has been designed from the ground up to be small, fast, and portable. At 53 megabytes, it can fit onto the smallest available (re-)writable CDs. Backing up a standard Windows 7 install takes 15 minutes or less, and restoring the same image can be done in 5 minutes. Finally, you can clone SEL BaRT to a USB flash drive for ultimate portability. Then simply take your USB flash drive with your cloned BaRT and any of your backup images, and you’ll be ready to restore.

SEL BaRT is custom-developed by SEL using open-source technology and is provided free of charge.

Installation Instructions

If you are using Windows 7, you may simply double-click the .iso file, then follow the onscreen instructions to begin the image burning process using the built-in Windows Disc Image Burner application.

For earlier versions of Windows or other operating systems, download the application guide for detailed instructions on creating an SEL BaRT CD.

SEL BaRT CD ISO

Version 3.3
Size 52.93 MB
Date Code 20160727

Verifying SEL Software Downloads

SEL Virtual Port Software

Transform unsecured serial or legacy Ethernet communications on Windows computers to cryptographically secure channels by using SEL-5827 Virtual Connect Client or SEL-5828 Virtual Port Service Software. These applications are provided free by SEL to make remote SEL-3620 Ethernet Security Gateway ports available for existing software and terminal applications on your PC, including those using Modbus TCP/RTU.

Notes

The SEL Virtual Port Software family includes the following applications:

  • SEL-5827 Virtual Connect Client—Create a temporary serial COM port or Ethernet TCP port for engineering access applications with the SEL-3620 and SEL-3622 Security Gateways.
  • SEL-5828 Virtual Port Service—Create multiple persistent serial COM ports or Ethernet TCP ports for automation applications.
SEL-5828 Virtual Port Service

  • Create up to 128 persistent virtual COM ports and/or virtual TCP ports on a Windows PC, and send serial data over Raw TCP, Telnet, and Secure Shell Protocol (SSH) Ethernet protocols.
  • Use DSA or RSA 1024-bit encryption with SSH to ensure confidentiality and authenticity for serial or Ethernet data.
  • Quickly create virtual serial or Ethernet ports with a simple user interface.
Version 1.3.0.0
Size 3.14 MB
Date Code 20160913

Verifying SEL Software Downloads

SEL-5827 Virtual Connect Client

  • Enhance the communications security of existing engineering access software solutions, such as SEL-5010 Relay Assistant Software, SEL-5020 Settings Assistant Software, and GE EnerVista™ software by converting serial and unencrypted TCP data to SSH.
  • Run on isolated SEL computers—SEL virtual port software does not connect to the Internet or require a license to run.
  • Back up virtual port configurations for quick commissioning of new computers and redundancy.
  • Use the built-in terminal window to interact with remote devices’ command-line interface.
Version 1.3.0.0
Size 3.49 MB
Date Code 20160913

Verifying SEL Software Downloads