Transmission

Traveling-Wave Fault Locating

SEL offers the only protective relays that include a traveling-wave-based fault locator, which is accurate to within a single tower span.

Field-proven SEL traveling-wave fault-locating technology calculates fault locations by measuring the arrival times of the naturally occurring traveling waves caused by a transmission line fault.This method provides much greater accuracy than traditional impedance-based methods. On a 300 km line, for example, impedance-based fault locating (typically accurate to about 2 percent of the line length) would require the visual inspection of approximately 6 km of the line. Traveling-wave-based fault locating in SEL relays can estimate the fault location to within 300 m (1,000 ft), independent of the line length—about one tower span for the typical overhead transmission line.

Locate Transmission Line Faults Quickly and Accurately

There are two distinct methods that can be used for traveling-wave fault locating:
  • Single-ended, for applications without a communications channel.
  • Double-ended, which requires two devices with communications.
SEL devices with traveling-wave fault locating also include a backup impedance-based fault locator to ensure dependable fault locating in the widest possible range of operating conditions and fault types.

Single-Ended Traveling-Wave Fault Locating

The single-ended traveling-wave method uses a single device to identify the first traveling wave and several successive traveling-wave reflections. It then calculates a prioritized list of possible fault locations.This method is useful in applications without device-to-device communications or when your communications channel is down.

Double-Ended Traveling-Wave Fault Locating

The double-ended traveling-wave method precisely measures the first traveling-wave arrival times at both line terminals and uses time synchronization between the two devices to calculate the fault location.Double-ended traveling-wave fault locating can be applied to two-terminal lines, including overhead lines, cable lines, and hybrid lines with a combination of overhead and cable sections. On series-compensated lines, the double-ended traveling-wave method provides more accurate results than the single-ended method.When applied to hybrid lines with overhead and cable sections, the double-ended traveling-wave fault locating in the SEL-T400L Time-Domain Line Protection and SEL-T401L Ultra-High-Speed Line Relay compensates for line nonhomogeneity, improving the accuracy of the results. The fault location is made available to the relay’s adaptive autoreclose cancel (ARC) logic in less than 60 ms and is then compared with user-defined settings to either block or allow reclosing.You can apply SEL devices with traveling-wave fault locating to multiterminal lines by obtaining the time stamps of the traveling waves that arrive at each end and using them in custom calculations in your SCADA/HMI software.

Improve System Reliability and Safety

The superior speed and accuracy of traveling-wave methods can facilitate advanced control functions that reduce the time and cost of repairs, mitigate potential property damage, and improve the safety of utility personnel and the public.

Control Autoreclosing on Hybrid Lines

SEL traveling-wave fault locators provide the fault type and an accurate fault location within milliseconds, which facilitates adaptive control of autoreclosing.Use double-ended traveling-wave locating with ARC logic to:
  • Adaptively control autoreclosing and single-pole tripping by asserting a control bit based on the fault location obtained at the line terminals.
  • Allow single-pole tripping and reclosing for faults on overhead line sections.
  • Force three-pole tripping and inhibit autoreclosing for faults on cable sections.

Implement Line Monitoring for Condition-Based Maintenance

SEL traveling-wave devices with the line-monitoring function allow you to obtain a location-tabulated event count to keep track of low-energy activity and faults along the line. Having identified problem locations based on event counts from the line-monitoring feature, you can prevent faults by selectively cleaning or replacing insulators, trimming vegetation, improving conductor antigalloping solutions, applying line spacers, or improving lightning protection. 

Analyze Ultra-High-Resolution Transient Recordings

The SEL-T400L and SEL-T401L relays and the SEL-TWFL Dual Traveling-Wave Fault Locator include ultra-high-resolution transient recording that captures current and voltage data at a 1 MHz sampling rate. With SEL-5601-2 Synchrowave Event Software, you can download the current and voltage data to visualize the timing of the initial and reflected traveling waves in a Bewley diagram and confirm the fault location.You can also use the recording function to analyze high-frequency transients from line energizations, switching events, circuit breaker restrikes (or reignitions), and self-extinguishing faults.  

Traveling-Wave Fault-Locating Products

SEL-T401L Ultra-High-Speed Line Relay

The SEL-T401L delivers subcycle operating times and includes a complete suite of primary and backup line protection functions, plus line monitoring, high-resolution event reporting, and traveling-wave fault locating that pinpoints faults to the nearest tower span.
  • Ultra-high-speed protection based on field-proven SEL time-domain technology with demonstrated trip times on the order of 1–5 ms.
  • Advanced distance elements, dependable and sensitive directional elements, and overcurrent elements for a complete protection solution.
  • Single-ended and double-ended traveling-wave fault locating.
  • Traveling-wave fault locating that allows adaptive autoreclosing to better protect hybrid lines.
  • Line-monitoring function for incipient faults, recurring faults, or incipient cable faults.
  • Recording and analysis of fault and system events, such as switching, breaker reignition, and self-extinguishing faults.
Learn more 

SEL-TWFL Dual Traveling-Wave Fault Locator and 12-Channel MHz Recorder

The SEL-TWFL delivers a fault location accuracy of one tower span, reducing the time and effort needed to find faults. It also includes line monitoring for condition-based line maintenance and high-resolution event reporting to analyze power system transients.
  • Pinpoint faults to the nearest tower span with traveling-wave fault locating.
  • Locate faults with single-ended and multi-ended traveling-wave and impedance-based methods.
  • Monitor the line for incipient faults, recurring faults, or incipient cable faults using the line monitoring function.
  • Complement protective relays by adding a standalone fault locator for two- and three-terminal lines.
  • Monitor as many as two lines at a substation using one device.
  • Record and analyze faults and system events, such as switching, breaker reignition, and self-extinguishing faults.
Learn more 

SEL-T400L Time-Domain Line Protection

Improve the reliability of your system with the high-speed operation and increased fault location accuracy of the SEL-T400L.
  • Secure tripping with ultra-fast reaction times to cover the gaps in traditional protection—without overtripping.
  • Fault locating—traveling-wave fault locating pinpoints faults to the nearest tower span.
  • Line-monitoring function for incipient faults, recurring faults, or incipient cable faults.
  • Recording and analysis of faults and system events, such as switching, breaker reignition, and self-extinguishing faults.
  • Protection upgrades—simple settings, a convenient 3U chassis, and SEL configuration and integration tools make it easy to replace existing relays.
Learn more 

Engineering Services

Let us partner with you to create an SEL solution for your system. From engineering studies and system design through commissioning and training, SEL engineers bring inventiveness and a deep understanding of the fundamental principles of electric power systems to every project. No matter how complex or sophisticated the system, we can help you protect, simplify, and control it.

Products and Service You Can Rely On

SEL products are designed and manufactured for the world’s most challenging environments, exceeding all industry standards for temperature, shock, and electric stress. An optional conformal coating for circuit boards adds an extra level of protection against contaminants in extreme environments.Every SEL product comes with a ten-year warranty—the best in the industry. If any product fails under warranty, we’ll repair or replace it for free.

Questions? Contact Us!

If you have any questions about SEL products, services, solutions, or support, please contact us. Our service and support professionals are ready to provide the answers you need.

Unbeatable Support

SEL support teams are stationed in regional offices around the world and staffed with application engineers who are experts in our products and in power system applications.

Technical support for SEL-manufactured devices is always complimentary. No matter how often you need to call or how long your SEL products have been in service, you’ll reach an SEL expert who can provide the service and support you need.

Our cybersecurity team is always ready with the information and resources needed to keep your OT networks and critical systems secure and working effectively. Cyber services support contracts can include incident response, audits, system hardening, and more, depending on your anticipated needs.

More about SEL warranty and support