SEL recently launched improvements to the website navigation menu!
Learn more about the enhancements.
Dismiss
Products
Industries
Services
Education
Support
Company
Login
SEL-3505/3505-3
Overview
Documentation
Support
SEL-3505/3505-3
Toggle Dropdown
Overview
Documentation
Support
Documentation
Featured
Instruction Manual
SEL-3505/SEL-3505-3 Automation Controller and
acSELerator
RTAC SEL-5033 Software
Data Sheet
SEL-3505/SEL-3505-3 Real-Time Automation Controller (RTAC)
Flyer
SEL-3505/3505-3 Real-Time Automation Controllers (RTACs)
Literature
Documents sorted by newest first.
Include English Literature
Literature
Flyers
Featured
SEL-3505/3505-3 Real-Time Automation Controllers (RTACs)
SEL Real-Time Automation Controller (RTAC) Product Family
Human-Machine Interface (HMI) for SEL Real-Time Automation Controllers (RTACs)
Secure Communications and Control Solutions
Automated NERC PRC-005 Maintenance and Testing
Grid Connect
Example Secure Control System Diagram
CAISO Remote Intelligent Gateway RTAC Flyer
Modern Water Delivery Solutions
Data Sheets
SEL-3505/SEL-3505-3 Real-Time Automation Controller (RTAC)
Guideform Specifications
SEL RTAC (3505, 3530, 3530-4, 3532, 3555, 2240) Guideform Specification
SEL RTAC (3505, 3530, 3530-4, 3532, 3555, 2240) Guideform Specification
Installation Guides
Getting Started With the SEL-3505/SEL-3505-3
Instruction Manuals
SEL-3505/SEL-3505-3 Automation Controller and
acSELerator
RTAC SEL-5033 Software
Certificates
SEL RTACs MICS
SEL RTACs PICS
SEL RTACs PIXIT
SEL RTACs TISSUES
SEL RTACs DNP3
RTAC IEC 61850 Edition 2 Certificates
Publications
Application Guides
SEL Fiber-Optic Device Compatibility Guide
Parsing the GPS Location in GPS NMEA Data From a Sierra Wireless RV55 Cellular Modem by Using RTAC Flex Parsing
Understanding and Using Static Routes in the SEL RTAC
Implementing Communication Redundancy in the RTAC
Related Material
RTAC Redundancy Projects
RTAC Redundancy Appendix A Projects
Using IEC 60870-5-103 Protocol Between the SEL Real-Time Automation Controller and SEL-751 Relays and Siemens SIPROTEC 7SJ80 Relays
Monitor IEEE 519 and 1547 Harmonic Distortion Levels With an SEL-735 and RTAC
Related Material
XML_Files
Retrieving Event Files From the RTAC by Using File Transfer Protocol
Managing IED Passwords With the SEL-3620 Ethernet Security Gateway and SEL RTAC Using SEL Server Connections
Understanding and Using Functions and Function Blocks in the RTAC
Configuring the SEL RTAC to Exchange Data With SEL IEDs Over IEC 61850 GOOSE
RTAC–IEC 61850 MMS Client-Server
Using SEL Fast Message Protocol Between the SEL-3530 RTAC and the SEL-2032
Using Flex Parsing in the RTAC With SEL Protocol to Obtain Energy Metering Data
SEL Fiber-Optic Communications Device Specifications
Configure the RTAC to Obtain Temperature Measurements From SEL Relays Via Flex Parse Messaging
Detecting a Loss of Communication Between an RTAC and a Relay
Configuring the SEL-3530 RTAC to Obtain Temperature Measured Using the SEL-2600
Defining DCE and DTE: Null Modem Cable and Straight-Through Cable Applications
Tiered Communication Between Remote Locations Using Multiple SEL-3530 RTACs
Automating Common RTAC Maintenance Tasks Using Python Scripts and SEL Software
Related Material
Python Scripts-AG2020-08
Using Wireshark to Troubleshoot Protocol Communications Issues on an RTAC
Using an RTAC to Get Three-Phase Fault Currents From SEL-400 Series Relays
Understanding and Effectively Using the SEL
Mirrored Bits
Protocol
Event Collection From SEL-3530 RTAC Using Team
SEL RTAC Axion Batch Sequencing With HMI for Industrial Automation Using Ladder Logic
Implement Serial DF1 Client Protocol in an RTAC By Using an
acSELerator
RTAC Extension
Related Material
DF1 Client
Using Breaker and Remote Bits to Implement Controls Through DNP3 From an RTAC HMI
Using an RTAC to Monitor Network Status With SNMP
Using an RTAC to Monitor and Report Firmware and Settings Changes in SEL Relays
Using Syslog to Report SEL Relay Security Status
Using an RTAC to Monitor GOOSE Statistics on SEL Relays
Using an SEL RTAC to Integrate the SEL-T400L Relay With SCADA
Maximizing RTAC Performance
Configuring an RTAC for a Typical SCADA Application
Setting the Modbus User Map on the SEL-734 and SEL-735 Meters Using the RTAC and FileIO Library
Related Material
UserMap
UserMap Spreadsheet
Integrating Fast Controls With SCADA Operations in the RTAC
Proportional Integral Derivative Controller Tuning for the Real-Time Automation Controller (RTAC) Platform
Convert SEL Fast Message Synchrophasor Messages to IEEE C37.118 Using the RTAC
Using Wireshark to Decode RTAC Serial Line Messages and SEL Protocols
Managing Time in the RTAC
Using the SEL-3505 Accelerometer and Light Sensor for Physical Security Monitoring
Using an RTAC to Read and Write Analog Data Values to an SEL-2411 Using SEL Fast Message Protocol
Using the SEL-3505 and SEL-3505-3 for Protocol Conversion and Monitoring
Basic and Advanced Applications of the SEL-3530 RTAC Access Point Router
Using an RTAC to Automatically Manage the Date and Time in Legacy Relays
Application Notes
IEC 61131-3 Variable Usage and Initialization in the RTAC
Registro de eventos analógicos en base de datos a través de los RTAC de SEL
Using Network Global Variable List Communications in Decentralized Control Solutions
Using the RTAC as a Modern Serial Data Line Analyzer
Open Channel Flow Control Using the SEL-2411, SEL-3031, and RTAC
Distributed Data Acquisition Using the SEL-2411 PAC and SEL-2440 DPAC
Power Plant - Steam Control
Adding Radio Pilot Channels and Backing Up SCADA Communications
Solar Tracking Using the SEL-2411 PAC and SEL-3530 RTAC
Use Synchrophasors in SCADA/EMS
Control Rotary Assembly Table Systems With SEL Automation Products
Case Studies
NREL Selects SEL Microgrid Controller for the Energy Systems Integration Facility
Technical Papers
Wind Farm Volt/VAR Control Using a Real-Time Automation Controller
White Papers
Best Practices for Implementing PTP in the Power Industry
Using Defense in Depth to Safely Present SCADA Data for Read-Only and Corporate Reporting
Automating Protection System Monitoring and Verification With the SEL RTAC
Leveraging Security – Using the SEL RTAC's Built-In Security Features
Drawings